Bus-off detection in TJA1043

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Bus-off detection in TJA1043

342 Views
Sam23
Contributor I

Dear Team,

Iam using TJA 1043 CAN transceiver, and I wanted to understand whether the transceiver can detect Bus-off in the following use case,
1. CANH open
2. CANL open
3. CANH and CANL open

Thanks

Tags (2)
0 Kudos
2 Replies

320 Views
Sam23
Contributor I

Thanks David for the detailed information.

0 Kudos

328 Views
diazmarin09
NXP TechSupport
NXP TechSupport

Hello Sam,

I hope all is great with you. Thank you for using the NXP communities.

The TJA1043 can detect short circuits on the bus wires and signal them to the host microcontroller. While physical bus failures normally lead to interruption of bus communication, there are certain bus failures that are tolerated within the physical layer of high speed CAN.

The system fail-safe features of the TJA1043 aim to keep the impact of possible local failures, like pin short-circuits, confined to the corrupted node only. After detection of a local failure, appropriate measures are taken to keep the remaining bus operable as long as possible. There are protections against TXD Dominant Clamping, TXD/RXD Short Circuit and Bus Dominant Clamping.

Please review the document below for further information, specially the chapter 7.4.

AH1014 - Application Hints - Standalone high speed CAN transceiver

I hope this information helps.

Regards,

David

0 Kudos