Bluetooth audio streaming using MKW36 board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Bluetooth audio streaming using MKW36 board

Jump to solution
1,999 Views
Anagha
Contributor I

Hello,

Can we use BLE of MKW36 board to audio streaming like message alert tone or incoming call or playing music by connecting our mobile phones? If so, please help me.

@bluetoothlowenergy 

Thanks and regards,

Anagha

Tags (1)
0 Kudos
Reply
1 Solution
1,987 Views
nxf56274
NXP Employee
NXP Employee

Hi,

The kw series doesn't support the audio streaming. Our NXH360 will support. You can refer this product.

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
6 Replies
1,988 Views
nxf56274
NXP Employee
NXP Employee

Hi,

The kw series doesn't support the audio streaming. Our NXH360 will support. You can refer this product.

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply
1,931 Views
Anagha
Contributor I

hello,

Is it not possible to audio stream over Bluetooth of MKW36 board or is it impossible to connect the external speakers to this MKW36 board? 

Please clarify this. @nxf56274 

Regards,

Anagha 

0 Kudos
Reply
1,920 Views
nxf56274
NXP Employee
NXP Employee

It is impossible to use mkw36 for audio stream.

0 Kudos
Reply
1,971 Views
Anagha
Contributor I

Hello,

Thank you for replying.

    What can be the source files? Can you please help me with this?

Do you have the source code or reference code regarding the same ? Can you please share the link of code and the related documents?  @nxf56274 

Regards,

Anagha

0 Kudos
Reply
1,940 Views
nxf56274
NXP Employee
NXP Employee

Hi,

All the material is in our website including the code and design file.

0 Kudos
Reply
1,930 Views
Anagha
Contributor I

Hello,

Sure, will go through this. 

Thanks for providing the link.

But is it not possible to Audio stream over bluetooth of MKW36 or is that we cant connect to the speakers to the MKW36 board? 

Please clarify this. @nxf56274 

Thanks and regards,

Anagha

0 Kudos
Reply