Hello,
Can we use BLE of MKW36 board to audio streaming like message alert tone or incoming call or playing music by connecting our mobile phones? If so, please help me.
@bluetoothlowenergy
Thanks and regards,
Anagha
解決済! 解決策の投稿を見る。
Hi,
The kw series doesn't support the audio streaming. Our NXH360 will support. You can refer this product.
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hi,
The kw series doesn't support the audio streaming. Our NXH360 will support. You can refer this product.
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
hello,
Is it not possible to audio stream over Bluetooth of MKW36 board or is it impossible to connect the external speakers to this MKW36 board?
Please clarify this. @nxf56274
Regards,
Anagha
It is impossible to use mkw36 for audio stream.
Hello,
Thank you for replying.
What can be the source files? Can you please help me with this?
Do you have the source code or reference code regarding the same ? Can you please share the link of code and the related documents? @nxf56274
Regards,
Anagha
Hi,
All the material is in our website including the code and design file.
Hello,
Sure, will go through this.
Thanks for providing the link.
But is it not possible to Audio stream over bluetooth of MKW36 or is that we cant connect to the speakers to the MKW36 board?
Please clarify this. @nxf56274
Thanks and regards,
Anagha