Hi,
I am doing some basic simulation of AFT27S010N transistor in ADS and I have some questions.
First, I am simulating IV curves. This is the schematic:

With this schematic, after launching simulation, I get the following warning:

Is there something wrong in my schematic? How can I avoid such warning?
Ignoring this warning, I go on with simulation. IV curves seem to be ok. For Vdc = 28v and Vgs = 1.9v, I get Ids = 112mA, which is near the 90mA used along the datasheet.

After that, I use another schematic to get S(2,1). In this schematic I set Vds = 28v and Vgs = 1.9v.

The values for S(2,1) are just a few dB, far from the about 20 dB stated in the datasheet.

Is there something wrong with the setup of my simulation?
Any advice will be very welcome.
I have attached the workspace I am using.