I download Autosar 4.3 driver for SJA1105 from the official website. I can't find the file named EthTrcv_43_TJA110X.h after install the software.At the same time, some macro definitions in file EthTrcv.h can not be found.I guess the sofeware package is a lack of files. Where can I find these missing files.
What I've seen in the EthTrcv_TS_T2D35M20I4R0 package, is the EthTrcv.h includes Eth.h file, not EthTrcv_43_TJA110X.h. See below snapshot:
The sample, however, is looking for the EthTrcv_43_TJA110x.h. It's mentioned in the guideline for sample application, that if you want to try out with the sample, you need to download the SWTJA110X-ETHTRCV430_RTM_1_0_4 (ID: SWT110X-SETRC43I).
You can contact your local sales representative to get the package.
Hello,
Did you install this package: SWSJA1105X-ETHSWT430_RTM_2_0_4? If yes, then it should be based on ASR 4.2, not ASR 4.3
Best Regards,
Nam
I think you misunderstand my question.I have found the plugin of EthTrcv in the ASR 4.2. And the file named EthTrcv_43_TJA110X.h is included in EthTrcv.h. The file I couldn't find is EthTrcv_43_TJA110X.h