Are the BGA6489 and BGA6589 SiGe Based MMICS?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Are the BGA6489 and BGA6589 SiGe Based MMICS?

602 Views
rockhound21
Contributor I

Are the BGA6489 and BGA6589 SiGe Based MMICS? CMOS, Bipolar, or BiCMOS ?

Tags (4)
0 Kudos
Reply
1 Reply

507 Views
LPP
NXP Employee
NXP Employee

BGA6489 and BGA6589 are silicon Monolithic Microwave Integrated Circuits.

MMIC offer the combination of several silicon based bipolar transistors, resistors and capacitors to perform specific RF function. The BGA6x89 series of medium power gain blocks are resistive feedback Darlington configured amplifiers. Resistive feedback provides large bandwidth with high accuracy.


Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply