Hi, I am Louriz. I am here requesting for the additional dimension for the MPN: TDA2614U.
Based on the datasheet, it do not mentioned the dimensions for the certain portion. I have also attached the datasheet and the photo which I need dimension on. I need the information is for evaluation purpose. Would appreciated you could advised it. Thanks.
Hi Louriz,
The dimension of the “capture” image is:
Min = 0.82mm
Max = 1.035mm
And the dimension of the “capture 1” is not characterized and cannot be calculated with the existing data.
Have a great day,
Jose
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------