Adapting PN5180 according to EMV BOOK-D. (Stage: Half-Duplex Block Transmission Protocol)

cancel
Showing results for 
Search instead for 
Did you mean: 

Adapting PN5180 according to EMV BOOK-D. (Stage: Half-Duplex Block Transmission Protocol)

101 Views
EkArge
Contributor II

I need some code samples for the PN5180 reader. For example the following example describing the Anticollosion phase (https://www.nxp.com/design/software:SOFTWARE-CENTER#/home/query/pn5180/~filter~/relevance/0  -> Anticollision register layer for PN5180 (REV 1.1) ))

But for PN5180, "Half-Duplex Block Transmission Protocol"
I need an example of the " layer. This layer deals with communication after sending a RATS and PPS command to the PICC. For example sending a DESELECT command to the PICC after this step or sending an APDU wrapped with a PCB (1byte) and EDC(2 bytes) It is related to.

In short, how is the "Half-Duplex Block Transmission Protocol" described in EMV-D adapted for PN5180? Can you share a pseudocode about it?

Note:
For EMV-D Half-Duplex Block Transmission Protocol: https://www.emvco.com/wp-content/uploads/2017/04/D_EMV_Contactless_Communication_Protocol_v2.6_20160... ( page: 217)

Labels (1)
  • RF

Tags (3)
0 Kudos
1 Reply

90 Views
fangfang
NXP TechSupport
NXP TechSupport

Hello @EkArge .

Thanks for your information.

For PN5180 we provide the library for the customer's application.  For the more information please kindly refer to the link. URL:https://www.nxp.com/design/designs/nfc-reader-library-software-support-for-nfc-frontend-solutions:NF....

 

Have a nice day.

 

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

0 Kudos