A problem occurred while attempting CAN function. The STB pin connected to the PTA 18 pin of S32K314 does not drop to 0V even if the signal is LOW. Given a LOW signal, the STB pin measures a voltage of approximately 1.9V. Also, even if R3 is removed and the circuit is cut off, the STB pin measures a voltage of approximately 0.7V, so the STB cannot be dropped to zero.
I understand that CAN IC operates when STB pin is below 0.3V and enters standby mode when STB pin is above 0.7V, am I correct in my understanding?
Please advise me to use it in NORMAL mode.
If CAN_STB is given a HIGH signal rather than LOW, the voltage of the STB pin is approximately 4.1V.
Hi,
The STB pin has an internal pull-up to VCC which creates a voltage divider with your resistor R4 resulting in a voltage drop on it.
Logic levels of the STB pin are defined in the datasheet. VIH min = 0.7 x VCC = 3.5V, VIL max = 0.3 x VCC = 1.5V.
BRs, Tomas
Hi,
Yes, if you connect the STB pin directly to GND, the device will be in the Normal mode and will not be able to enter the Standby mode.
BRs, Tomas