About CAN Wakeup Pulse in MC33742

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About CAN Wakeup Pulse in MC33742

768 Views
vinman0261
Contributor I

Folks,

Using MC33742 (SBC - CAN Transceiver - 28 pin IC) in one of our project.

Initialized the Transceiver in Normal mode. After 100 milliseconds of Power up, CAN TX (Pin# - 2) is getting reset.

Due to this reset pulse, we couldn't able to transmit data via CAN bus. Attached the evidence for the same.

Can anyone tell me how to resolve this issue.

Thanks

Vinoth

0 Kudos
Reply
2 Replies

627 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

It is being solved internally (Case 00151731).

0 Kudos
Reply

628 Views
andrea_costa
Contributor I

Hi Tomas,

i'm facing the same issue :smileysad: The SPI init sequence is the one suggested in the datasheet (DEBUG MODES WITH SOFTWARE WATCHDOG DISABLED THOUGH SPI) and i'm sending via SPI the commands  {0xB5, 0x10, 0x15, 0x5F}.

What i'm missing? How did you manage to solve the problem?

Thanks,

Andrea

0 Kudos
Reply