AN636A data sheet shows RF input resistance 700Ohm and RF input capacitance 3.5pf at 240Mhz. Can I assume these are in parallel. How is this information useful when trying to match at other frequencies? Is there an input impedance versus frequency chart some where for the AN636? I have seen them for the 605A and 606A. I want impedance for 120Mhz. Thanks
RFi single-ended input capacitance of SA636 is provided relative to GND. It is parallel to input resistance.
Matching circuit in Figure 15 is suitable for 120MHz (for good RLI about -20dB).
Have a great day,
Pavel
NXP TIC
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------