AN636A input impedance versus frequency chart

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

AN636A input impedance versus frequency chart

998 Views
mattfindlow
Contributor II

AN636A data sheet shows RF input resistance 700Ohm and RF input capacitance 3.5pf at 240Mhz. Can I assume these are in parallel. How is this information useful when trying to match at other frequencies? Is there an input impedance versus frequency chart some where for the AN636?  I have seen them for the 605A and 606A.  I want impedance for 120Mhz. Thanks

Labels (1)
  • RF

0 Kudos
Reply
1 Reply

816 Views
LPP
NXP Employee
NXP Employee

RFi single-ended input capacitance of SA636 is provided relative to GND. It is parallel to input resistance.

Matching circuit in Figure 15 is suitable for 120MHz (for good RLI about -20dB).

Have a great day,
Pavel
NXP TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply