A3I20X050GN LDMOS PA FET VGGC parameter clarification

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

A3I20X050GN LDMOS PA FET VGGC parameter clarification

Jump to solution
752 Views
louissankoorika
Contributor I

Hi,

We are using the A3I20X050GN LDMOS PA FET in our design.

I need clarity on the VGGC(Q) parameter

Fixture Gate Quiescent Voltage, (VDD = 28 Vdc, IDQ(Carrier) = 160 mAdc, Measured in Functional Test),
VGGC(Q)

How  is it different from VGSC(Q) parameter which is also specified?

Gate Quiescent Voltage (VDS = 28 Vdc, IDQ(Carrier) = 160 mAdc) VGSC(Q)

Thanks

Louis

Labels (1)
  • RF

0 Kudos
1 Solution
731 Views
andrei_skok
NXP Employee
NXP Employee

Gate Quiescent Voltage VGS(Q) is measured at the VGS pins of the device.
Fixture Gate Quiescent Voltage VGG(Q) is measured in test circuit at the VGG supply.

Temperature compensation circuit sinks the current. VGG(Q) differ from VGS(Q) by the voltage drop at the circuit bias resistors R3=10 Ohm, R1=2.2kOhm.

View solution in original post

0 Kudos
1 Reply
732 Views
andrei_skok
NXP Employee
NXP Employee

Gate Quiescent Voltage VGS(Q) is measured at the VGS pins of the device.
Fixture Gate Quiescent Voltage VGG(Q) is measured in test circuit at the VGG supply.

Temperature compensation circuit sinks the current. VGG(Q) differ from VGS(Q) by the voltage drop at the circuit bias resistors R3=10 Ohm, R1=2.2kOhm.

0 Kudos