I had the LPC54018-based loT Module board and LPC-Link2. I tried download the board,but could not.
The following actions of mine:
1:open the program LPC-LINK2 with CMSIS-DAP software. I entered one key,but An error occurred in this window.
The error:
LPCScrypt - CMSIS-DAP firmware programming script v2.0.0 June 2018.
Connect an LPC-Link2 or LPCXpresso V2/V3 Board via USB then press Space.
Press any key to continue . . .
Booting LPCScrypt target with "LPCScrypt_227.bin.hdr"
LPCScrypt target boot failed:
Invalid DFU suffix signature
A valid DFU suffix will be required in a future dfu-util release!!!
error get_status
.............
How can i solve the problem?
I think the problem causes i can not download.
Please help the problem as soon as possible.
Thans.
Hello 爱飞 张
After connecting the board to your pc through the debug probe you have to check that you have JP6 connected.
This is the process to update the firmware for this LPC:
Let me know if this helps you. Have a great day
Omar
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
-------------------------------------------------------------------------------
Hi Omar:
Thank you for your reply!
B/R
Aifei Zhang
发件人: nxf54944
发送时间: 2019年7月9日 7:51
收件人: Aifei Zhang
主题: Re: - Re: A problem of the LPC-LINK2
NXP Community <https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>
Re: A problem of the LPC-LINK2
reply from Omar Anguiano <https://community.nxp.com/people/nxf54944?et=watches.email.thread> in Other NXP Solutions - View the full discussion <https://community.nxp.com/message/1175137?commentID=1175137&et=watches.email.thread#comment-1175137>