56F8367 Downloading then "Core Not Responding"

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

56F8367 Downloading then "Core Not Responding"

ソリューションへジャンプ
1,675件の閲覧回数
Charlie
Contributor III
I have with me the 56F8367 eval board and our actual board with the same chip on it.

We have created our own little homemade parallel to JTAG converter cable to debug the chip on the board, but considering we have tried the cable on the JTAG connector on the eval board and it works, I doubt the cable is the problem.

We have checked GNDs, Vcc, and have even watched all of the JTAG signals to see if anything is happening.  We have messed around with a bunch of jumper settings but at this point we are struggling to find the answer.

The weird thing is that when we start to download, it appears to connect okay and the downloading progress bar message box appears in codewarrior for 1 tick and then immediately the message box "Core Not Responding" pops up.

I thought I would check here for any help before I issued a ticket.  Thanks to all.
0 件の賞賛
返信
1 解決策
906件の閲覧回数
Charlie
Contributor III
This problem has been solved.  The problem was that we had a bad pull-up resistor on the TDO line and so the data going back to codewarrior didn't look right.  Fixed the pull up resistor and everything works fine.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
907件の閲覧回数
Charlie
Contributor III
This problem has been solved.  The problem was that we had a bad pull-up resistor on the TDO line and so the data going back to codewarrior didn't look right.  Fixed the pull up resistor and everything works fine.
0 件の賞賛
返信