32Gbps MUX IC similar in functionality to CBTU02044

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

32Gbps MUX IC similar in functionality to CBTU02044

1,611 Views
lalit_verma
Contributor II

Hi,

We are in need of a high speed differential MUX similar to CBTU02044.

CBTU02044 supports PCIe Gen4 speed, but we need a MUX which can support data rate up to 32Gbps.

Does NXP has MUX IC similar to CBTU02044 functionality which can support data rate up to 32Gbps.

Thanks

Tags (1)
0 Kudos
Reply
3 Replies

1,562 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Lalit,

Unfortunately not. There are not currently any MUX, which would have higher bandwidth than the CBTU02044.

Best regards,

Tomas

0 Kudos
Reply

1,562 Views
lalit_verma
Contributor II

Tomas Vaverka wrote:

Hi Lalit,

 

Unfortunately not. There are not currently any MUX, which would have higher bandwidth than the CBTU02044.

 

Best regards,

Tomas

Hi Tomas,

Can u please share the IBIS-AMI model of CBTU02044.

We would like to perform a simulation of CBTU02044 for our application to check the maximum operating data rate of CBTU02044 so that we can check whether we can use CBTU02044 in our desing. 

Thanks,

Lalit

0 Kudos
Reply

1,562 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Lalit,

We do not have an IBIS model for the CBTU02044.

Usually customers use the S-parameter model for their high-speed channel simulation.

Attached please find the S-parameter model for the CBTU02044.

Best regards,

Tomas

0 Kudos
Reply