Hi,
We are in need of a high speed differential MUX similar to CBTU02044.
CBTU02044 supports PCIe Gen4 speed, but we need a MUX which can support data rate up to 32Gbps.
Does NXP has MUX IC similar to CBTU02044 functionality which can support data rate up to 32Gbps.
Thanks
Hi Lalit,
Unfortunately not. There are not currently any MUX, which would have higher bandwidth than the CBTU02044.
Best regards,
Tomas
Tomas Vaverka wrote:
Hi Lalit,
Unfortunately not. There are not currently any MUX, which would have higher bandwidth than the CBTU02044.
Best regards,
Tomas
Hi Tomas,
Can u please share the IBIS-AMI model of CBTU02044.
We would like to perform a simulation of CBTU02044 for our application to check the maximum operating data rate of CBTU02044 so that we can check whether we can use CBTU02044 in our desing.
Thanks,
Lalit