16 Channel Adjustable Constant Current LED Driver

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

16 Channel Adjustable Constant Current LED Driver

跳至解决方案
1,575 次查看
guitardenver
Contributor IV

I'm looking for a drop in replacement for the TI TLC5926IPWPR LED driver.

 

It's 16 channel constant current LED driver. Max current is set via an external resistor, but we can also adjust the current via the SPI interface.

 

Does NXP have this as well? I do not need error detection feature. Just need to adjust the current via SPI bus.

5mA to 61mA output current.

0 项奖励
回复
1 解答
1,535 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Matt,

There is not a drop in replacement for the TI TLC5926IPWPR currently available in our portfolio.

The closest device is the PCA9745B: 16-channel SPI serial bus 57 mA/20 V constant current LED driver:

https://www.nxp.com/docs/en/data-sheet/PCA9745B.pdf

There is a table with all NXP’s LED controllers available in the following document, page 3:

https://www.nxp.com/docs/en/brochure/LED-CONTROLLERS-FINAL-DELIVERABLES.pdf

Best regards,

Tomas

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,536 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Matt,

There is not a drop in replacement for the TI TLC5926IPWPR currently available in our portfolio.

The closest device is the PCA9745B: 16-channel SPI serial bus 57 mA/20 V constant current LED driver:

https://www.nxp.com/docs/en/data-sheet/PCA9745B.pdf

There is a table with all NXP’s LED controllers available in the following document, page 3:

https://www.nxp.com/docs/en/brochure/LED-CONTROLLERS-FINAL-DELIVERABLES.pdf

Best regards,

Tomas

0 项奖励
回复