用KEIL 给MKV46F256烧录不了程序

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

用KEIL 给MKV46F256烧录不了程序

23,090 Views
xiaobing_yin
Contributor I

使用的是官网下载的Demo历程,给MKV46F256烧录程序时,烧录不了,报错信息如下:

Full Chip Erase Done.
Programming Done.
Contents mismatch at: 0000001CH  (Flash=00H  Required=96H) !
Contents mismatch at: 0000001DH  (Flash=00H  Required=A6H) !
Contents mismatch at: 0000001EH  (Flash=00H  Required=FFH) !
Contents mismatch at: 0000001FH  (Flash=00H  Required=DFH) !
Verify Failed!
Error: Flash Download failed  -  "Cortex-M4"
Flash Load finished at 10:07:33

0 Kudos
Reply
9 Replies

22,839 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi bing yin,

我在TWR-KV46F150M板上测试SDK_2.6.0_MKV46F256xxx16\boards\twrkv46f150m\demo_apps\hello_world例程,能够使用JLink仿真器在此配置下进行debug。

Flash Download setup.png

你可以参考:Error: Flash Download failed - "Cortex-M4":Contents mismatch 里的提示查

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

22,838 Views
xiaobing_yin
Contributor I

您好,我现在有以下两个问题,需要咨询一下,如下

问题1: 问题1.在定时器配置时,我该如何计算频率。如下图所示。

问题2.在芯片引脚配置时,有个函数,如下图所示,其中参数kPort_MuxAlt6我该如何选择,kPort_MuxAlt2-kPort_MuxAlt15各代表什么意思?分别在那种模式下使用。

以上两个问题,还请务必回复一下,请知悉,谢谢!

在 2019-08-01 10:57:56,"Robin_Shen" <admin@community.nxp.com> 写道:

|

|

NXP Community

|

|

Re: 用KEIL 给MKV46F256烧录不了程序

reply from Robin_Shen in Other NXP Products - View the full discussion

Hi bing yin,

我在TWR-KV46F150M板上测试SDK_2.6.0_MKV46F256xxx16\boards\twrkv46f150m\demo_apps\hello_world例程,能够使用JLink仿真器在此配置下进行debug。

https://community.nxp.com/servlet/JiveServlet/downloadImage/2-1185571-274980/1186-900/FlashDownloadsetup.png

你可以参考:Error: Flash Download failed - "Cortex-M4":Contents mismatch 里的提示查

Best Regards,

Robin

0 Kudos
Reply

22,837 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

问题1.在定时器配置时,我该如何计算频率。如下图所示。
答1:FTM_SetTimerPeriod里既然调用了USEC_TO_COUNT,那么1000U这个位置(us)直接输入周期多少微秒就行了。
如果你想手动计算也行:period of counting = (MOD - CNTIN + 0x0001) x period of FTM counter clock
已知fast peripheral clock频率
且FTM counter clock经过4分频(你的图里第8行代码)
假设CNTIN=0
求MOD值(16位寄存器最大0xff)

period of counting.png


问题2.在芯片引脚配置时,有个函数,如下图所示,其中参数kPort_MuxAlt6我该如何选择,kPort_MuxAlt2-kPort_MuxAlt15各代表什么意思?分别在那种模式下使用。
答2:参考手册KV4XP100M168RM的“11.5 KV4x Signal Multiplexing and Pin Assignments”里查

KV4x Signal Multiplexing and Pin Assignments.png

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

22,837 Views
xiaobing_yin
Contributor I

您好。

关于PWM有各问题需咨询,代码配置如下:

示波器抓取的波形如下:

请问,波形为什么会是这样,低电平为什么不能完全拉低,该如何使低电平完全拉低?还请不吝赐教,谢谢!

在 2019-08-02 09:48:11,"Robin_Shen" <admin@community.nxp.com> 写道:

|

|

NXP Community

|

|

Re: 用KEIL 给MKV46F256烧录不了程序

reply from Robin_Shen in Other NXP Products - View the full discussion

问题1.在定时器配置时,我该如何计算频率。如下图所示。

答1:FTM_SetTimerPeriod里既然调用了USEC_TO_COUNT,那么1000U这个位置(us)直接输入周期多少微秒就行了。

如果你想手动计算也行:period of counting = (MOD - CNTIN + 0x0001) x period of FTM counter clock

已知fast peripheral clock频率

且FTM counter clock经过4分频(你的图里第8行代码)

假设CNTIN=0

求MOD值(16位寄存器最大0xff)

https://community.nxp.com/servlet/JiveServlet/downloadImage/2-1186294-275041/periodofcounting.png

问题2.在芯片引脚配置时,有个函数,如下图所示,其中参数kPort_MuxAlt6我该如何选择,kPort_MuxAlt2-kPort_MuxAlt15各代表什么意思?分别在那种模式下使用。

答2:参考手册KV4XP100M168RM的“11.5 KV4x Signal Multiplexing and Pin Assignments”里查

https://community.nxp.com/servlet/JiveServlet/downloadImage/2-1186294-275096/KV4xSignalMultiplexingandPin+Assignments.png

Best Regards,

Robin

0 Kudos
Reply

22,836 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

先找个其他信号源输出类似频率方波,通过示波器检查波形是否也会产生类似畸变。

然后测试官方例程(...\SDK_2.6.0_MKV46F256xxx16\boards\twrkv46f150m\driver_examples\pwm),查证readme提示引脚波形。

0 Kudos
Reply

22,836 Views
xiaobing_yin
Contributor I

你好。关于ADC我现在遇到问题,我这边移植的Demo,什么现象也没有,还会导致我其他的程序运行不正常(仿真时并未死机),代码见附件,还请帮忙查看一下,ADC配置是否正确。谢谢!

在 2019-08-05 11:00:40,"Robin_Shen" <admin@community.nxp.com> 写道:

|

|

NXP Community

|

|

Re: 用KEIL 给MKV46F256烧录不了程序

reply from Robin_Shen in Other NXP Products - View the full discussion

先找个其他信号源输出类似频率方波,通过示波器检查波形是否也会产生类似畸变。

然后测试官方例程(...\SDK_2.6.0_MKV46F256xxx16\boards\twrkv46f150m\driver_examples\pwm),查证readme提示引脚波形。

Reply to this message by replying to this email, or go to the message on NXP Community

Start a new discussion in Other NXP Products by email or at NXP Community

Following Re: 用KEIL 给MKV46F256烧录不了程序 in these streams: Inbox

This email was sent by NXP Community because you are a registered user.

You may unsubscribe instantly from NXP Community, or adjust email frequency in your email preferences

|

|

0 Kudos
Reply

22,836 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

鉴于回帖与主题偏离,建议你重新创建一个帖子提问。

我们的工程师会在新帖里帮你解答。

0 Kudos
Reply

22,834 Views
xiaobing_yin
Contributor I

Hi,

关于ADC,对于有些特殊得通道,ADC得通道号和函数void CADC_SetSampleConfig(ADC_Type *base, uint16_t sampleIndex, const cadc_sample_config_t *config)中得第二个参数sampleIndex得值如何让确定请告知。如使用ADCA_CH6A(pin14)时,则此时通道号和sampleIndex如何确定?代码片段如下

以上问题还请解答一下,谢谢!

在 2019-08-13 11:32:36,"Robin_Shen" <admin@community.nxp.com> 写道:

|

|

NXP Community

|

|

Re: 用KEIL 给MKV46F256烧录不了程序

reply from Robin_Shen in Other NXP Products - View the full discussion

鉴于回帖与主题偏离,建议你重新创建一个帖子提问。

我们的工程师会在新帖里帮你解答。

Reply to this message by replying to this email, or go to the message on NXP Community

Start a new discussion in Other NXP Products by email or at NXP Community

Following Re: 用KEIL 给MKV46F256烧录不了程序 in these streams: Inbox

This email was sent by NXP Community because you are a registered user.

You may unsubscribe instantly from NXP Community, or adjust email frequency in your email preferences

|

|

0 Kudos
Reply

22,834 Views
xiaobing_yin
Contributor I

您好!

我使用MKV46F256VLL16芯片,移植的Demo历程,ADC采集部分,现问题如下:ADC采集时,程序一直死在等待转换完成语句处,代码如下

关于ADC得配置部分代码如下:

以上问题,还请帮忙解答一下。谢谢!

|

|

|

|

0 Kudos
Reply