我已经将A1006成功挂载到i2c电路上,请问我如何检测电路是否工作.我可以在linux系统中使用i2cdetect和i2cdump命令,但是检测出来寄存器全是01,不太清楚,是否工作。
Hi,
It is not the right way with A1006, please kindly refer to Get Started with the KIT-A1006-Shield | NXP for details.
Hope that helps,
Have a great day,
Kan
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------