在lsdk2012下编译VPP v2005时生成的deb文件问题

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

在lsdk2012下编译VPP v2005时生成的deb文件问题

344 Views
jianghong
Contributor I

hi,

我在在lsdk2012下编译VPP v2005时生成的DEB文件为什么是:

libvppinfra_20.05.1-6~gf53edbc3b_amd64.deb vpp_20.05.1-6~gf53edbc3b_amd64.deb vpp-dev_20.05.1-6~gf53edbc3b_amd64.deb
libvppinfra-dev_20.05.1-6~gf53edbc3b_amd64.deb vpp-api-python_20.05.1-6~gf53edbc3b_amd64.deb vpp-plugin-core_20.05.1-6~gf53edbc3b_amd64.deb
python3-vpp-api_20.05.1-6~gf53edbc3b_amd64.deb vpp-dbg_20.05.1-6~gf53edbc3b_amd64.deb vpp-plugin-dpdk_20.05.1-6~gf53edbc3b_amd64.deb

而不是arm64呢?

编译命令:

flex-builder -c vpp -a arm64

编译端口错误:

Reading state information... Done
The following additional packages will be installed:
python3-cffi-backend python3-ply python3-pycparser
Suggested packages:
python-ply-doc
The following NEW packages will be installed:
python3-cffi python3-cffi-backend python3-ply python3-pycparser
0 upgraded, 4 newly installed, 0 to remove and 0 not upgraded.
Need to get 242 kB of archives.
After this operation, 1,352 kB of additional disk space will be used.
Err:1 http://us.ports.ubuntu.com/ubuntu-ports bionic/main arm64 python3-cffi-backend arm64 1.11.5-1
Could not connect to apac.nics.nxp.com:8080 (127.0.0.1). - connect (111: Connection refused)
Err:2 http://us.ports.ubuntu.com/ubuntu-ports bionic/main arm64 python3-ply all 3.11-1
Unable to connect to apac.nics.nxp.com:8080:
Err:3 http://us.ports.ubuntu.com/ubuntu-ports bionic/universe arm64 python3-pycparser all 2.18-2
Unable to connect to apac.nics.nxp.com:8080:
Err:4 http://us.ports.ubuntu.com/ubuntu-ports bionic/universe arm64 python3-cffi all 1.11.5-1
Unable to connect to apac.nics.nxp.com:8080:
E: Failed to fetch http://us.ports.ubuntu.com/ubuntu-ports/pool/main/p/python-cffi/python3-cffi-backend_1.11.5-1_arm64.... Could not connect to apac.nics.nxp.com:8080 (127.0.0.1). - connect (111: Connection refused)
E: Failed to fetch http://us.ports.ubuntu.com/ubuntu-ports/pool/main/p/ply/python3-ply_3.11-1_all.deb Unable to connect to apac.nics.nxp.com:8080:
E: Failed to fetch http://us.ports.ubuntu.com/ubuntu-ports/pool/universe/p/pycparser/python3-pycparser_2.18-2_all.deb Unable to connect to apac.nics.nxp.com:8080:
E: Failed to fetch http://us.ports.ubuntu.com/ubuntu-ports/pool/universe/p/python-cffi/python3-cffi_1.11.5-1_all.deb Unable to connect to apac.nics.nxp.com:8080:
E: Unable to fetch some archives, maybe run apt-get update or try with --fix-missing?
COMPONENT: dpdk

 

如何解决以上问题呢,请帮忙尽快回复,

谢谢

 

0 Kudos
Reply
0 Replies