哪一个硬件的定时器程序可以直接放到imx6d的板子上,进行运行、测试(Which hardware timer program can be directly put on the imx6d bo)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

哪一个硬件的定时器程序可以直接放到imx6d的板子上,进行运行、测试(Which hardware timer program can be directly put on the imx6d bo)

1,475件の閲覧回数
刘洋
Contributor III

目前在测试imx6d所在的电路板,但是定时器程序,虽说用的是C语言编写的,但是标志位什么的,自己编写了很多,但是没效果。特来请教,是否有研究imx6d的,能交流一下。谢谢

I am currently testing the circuit board where imx6d is located, but although the timer program is written in C language, I have written a lot of flags and so on, but it has no effect. I would like to ask if there is any research on imx6d, so I can exchange it. Thank you!

0 件の賞賛
返信
2 返答(返信)

1,472件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

请问你这里是自己做的板子吗?是否是参考NXP 开发板做的板子?如果是自己做的板子的话,你需要做BSP的移植, 不知道你要使用Linux 还是adroid 版本的BSP, 建议你参考我们官网提供的移植文档进行移植。

1,468件の閲覧回数
刘洋
Contributor III

嗯嗯,我是自己做的板子,然后,在板子上用到MCIMX6D7CVT08AE与FPGA两块芯片,目前是想写一个定时器LED闪烁的测试程序在IAR  FOR  ARM8.10中,win10系统中进行上述操作,希望能得到您的技术支持。谢谢

0 件の賞賛
返信