FXOS8700CQ Auto-sleep with Magnetic threshold trigger

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FXOS8700CQ Auto-sleep with Magnetic threshold trigger

FXOS8700CQ Auto-sleep with Magnetic threshold trigger

*********************************************************************************************************
* This simple example code has been written for the FRDM-KL25Z + FRDM-FXS-MULT2-B
* boards and demonstrates how to use the embedded magnetic threshold detection
* function in conjunction with the auto-wake/sleep mode for reducing current
* consumption of the FXOS8700CQ.
*
* The magnetic threshold is set to 100uT (1000 counts) on the X and Y axis.
* Once this threshold is exceeded, the FXOS8700CQ is waken up and an interrupt
* is generated on the INT1 pin. If the magnetic field is below this threshold
* within the 20ms period, the FXOS8700CQ goes back to sleep mode and also
* generates an interrupt on the INT1 pin.
*********************************************************************************************************

添付
評価なし
バージョン履歴
最終更新日:
‎10-01-2017 09:24 AM
更新者: