FRDM-A9957HN Evaluation Board

cancel
Showing results for 
Search instead for 
Did you mean: 

FRDM-A9957HN Evaluation Board

No ratings

FRDM-A9957HN Evaluation Board

**************************************************************************************************************
The FRDM-A9957HN is an EVB designed for evaluation of PCA9957 daisy-chain SPI-compatible 4-wire serial bus controlled 24-channel constant current LED driver optimized for dimming and blinking 32 mA Red/Green/Blue/Amber (RGBA) LEDs.

*

The FRDM-A9957HN is designed to be used with FRDM-KL25Z Freedom Development Platform and an SDK example code

*

* Connection:      FRDM-KL25Z           OM13513
* VDD                 J9-4                           J9-2                                                                                                           * VDDIO             J9-8                            J9-4
* GND                 J2-14                         J2-7
* MOSI               J2-8                            J2-4
* MISO               J2-10                          J2-5
* SCLK               J2-12                          J2-6
* CS                   J2-6                            J2-3
* RESET            J9-6                            J9-3
***************************************************************************************************************

JozefKozon_0-1633004398536.png

 

Labels (1)
Attachments
Version history
Revision #:
3 of 3
Last update:
‎09-30-2021 05:28 AM
Updated by: