which USBDM can support MC56F82748?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

which USBDM can support MC56F82748?

808 Views
wangbaode
Contributor IV

Hi pgo,

which USBDM can support MC56F82748?

Tags (2)
0 Kudos
3 Replies

520 Views
pgo
Senior Contributor V

Very belated reply.

USBDM V4.10.6.250 now supports this chip.

bye

0 Kudos

520 Views
wangbaode
Contributor IV

dear pgo,

thank you very much.

best regards for you

bye

0 Kudos

520 Views
fallanck
Contributor I

Hello, wang,

it seems, that (according the informations from the USBDM page - USBDM: USBDM Debugger interface for Freescale RS08,HCS08,HCS12,Coldfire and ARM-Kinetis Devices.) the DSC support is for the "M56F80xx only", and in the table about the various USBDM hardwares there is a note: "DSC support is very limited in Codewarrior 10 and the stand-alone programmer".

We are using this DSC in our design and we made some  USBDM_CF_JMxxCLD_V3, which are used in our development process, mostly with HCS08 chips. It could be nice to have support for this DSC in USBDM.

So there is a question for pgo: is there any possibility to add support for the MC56F82748 DSC?

I don't know the reasons why this DSC is not supported. Maybe there are technical reasons and maybe simply there was no need to add the support yet as most people uses USBDM with HCS08 and Kinetis processors.

regards,

Miklos

0 Kudos