Using libusb 0.1.2.6. TestLibUsb reports dll version 0.1.2.6, driver version -1.-1.-1.-1, and that's the problem. tryUSBDM finds 1 bus with no devices even though device manager says there are 2. HiWave debugger in Legacy Codewarrior has no issues. What (where) is the missing driver? I admit that tryUSBDM is ancient but it interfaces the bus using libusb api's.
Hi Laurence,
Sorry but I find your question very confusing and have only the vaguest memory of tryUSBDM although I presume it has to do with USBDM :smileyhappy:.
I have no real idea what you are asking but it may be useful to note that USBDM changed to libusb-V1 around V4.9.3 (March 2012) from libusb-win32 (libusb-V0.1) so this may account form some of your mixed results. It also changed the PID/VID along the way.
If you are using an old enough BDM it may actually be 'pretending' to be a TBDML. So all round it can be very confusing.
What exactly are you trying to do?
What software are you using (including version - do you actually mean 4.6.10.220 or 4.10.6.220?)
What hardware?
bye