Unable to detect microcontroller in CodeWarrior

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Unable to detect microcontroller in CodeWarrior

1,006 Views
kpro3
Contributor I

I have a KITMMA955XLEVM: Sensor Toolbox for Xtrinsic Smart Sensing Platform, and using CodeWarrior 10.2.

I am trying to create a custom program and load it on to the microcontroller. However, I am unable to connect or even find the microcontroller when attempting to enter debug mode.

osbdm.jpg

I'm running a Bareboard Project with Open Source BDM. The board is connected to the computer through a single USB cable. I am able to use Sensor Toolbox to read the data from the board. The CPU type on the board is MCF51QE64CLH.

I am running on Windows 7 Home Premium 64-bit. I've tried re-installing the drivers from PEMicro.com, but nothing shows up in Device Manager.

osbdm2.jpg.png

Any help or advice would be greatly appreciated. Cheers.

Labels (1)
0 Kudos
Reply
0 Replies