USBDM problem using CodeWarrior 6.3 in windows vista x86

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USBDM problem using CodeWarrior 6.3 in windows vista x86

1,174件の閲覧回数
mandres
Contributor I

Hi, I am using an open source USBDM JM60 and I am trying to program a MC9S08JM 16, when I click on debug,  CodeWarrior displays a lot of warning messages and nothing happens with the microcontroller, this is not programmed at the end. I attached the screenshots of the warning messages, I do not know what's going on, I hope someone can help me.

The USBDM is recognized perfectly by the computer like a Libusb-win32 device.

ラベル(2)
タグ(2)
0 件の賞賛
返信
1 返信

356件の閲覧回数
pgo
Senior Contributor V

Dear mandres,

 

What version of USBDM firmware and software?

Have you actually installed the DLL files?

Do you get the USBDM connection dialogue?

 

No suggestions are possible without the above information.

 

The dialogue provided don't really indicate much unfortunately - Just that codewarrior is having problems connecting to the target.

 

bye

 

0 件の賞賛
返信