USBDM issue - not support target

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USBDM issue - not support target

1,141 Views
WebberS
Contributor I

Hi,

    I am working with MC9S12XEP100. And I tred to mass erase the flash of this chip by USBDM. But it showed an error 'USBDM interface does not support target device'. Also, there is no MC9S12XEP100 series chips could be select manually. The USBMD works if I linked it by debuging through CodeWarrior. Could you help to check if any other configure should I do to enbale the interface support MC9S12XEP100 chips?

      Error mesage is also uploaded. USBDM version is 4.12.1.340. FIrmware version is 4.12.1.

WebberS_0-1744600932718.png

WebberS_1-1744600958413.png

 

 

Tags (1)
0 Kudos
Reply
0 Replies