USBDM install/run problem with Ubuntu 16.04 LTS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USBDM install/run problem with Ubuntu 16.04 LTS

1,360 Views
jpa
Contributor IV

I know it's brand new software, but as it's the latest LTS, maybe we can get a jump start on it? 

 

The package installation of 4.12.1.70-1.amd64.deb failed.  Running it in the command line showed a couple of missing dependencies, one of which was resolved (off screen), another which was resolved in the attached log of the install process.  With the dependencies fixed, it seems to install, but running the ARM_FlashProgrammer yields the fault shown in the attached PNG file. 

 

The whole thing is running in a VirtualBox VM (Ubuntu 14.04 host).

As an aside, I'm a bit concerned that it seems to be installing plugins from an Eclipse MARS repository, when I have Kepler installed (because it seemed as if some other ARM/Kinetis software was better supported for Kepler, not even Luna). 

Another concern that it seems to be installing them also in "/opt/eclipse_was" which is how I thought I was hiding that directory from changes...by adding the "_was". 

 

Going back to 4.10.6.240 doesn't seem to help because there are dependencies on a 2.8 version of a library, and Ubuntu seems to stubbornly insist on providing 3.0. 

 

Thanks in advance for any help you can provide...

 

John

Original Attachment has been moved to: log_from_usbdm_4.12.1.70-amd64.deb.txt.zip

0 Kudos
Reply
1 Reply

1,003 Views
michaelheidinge
Contributor III

I can confirm, that ubuntu 16.04 lts has some issues here, too. I cannot install it too. I too would apprechiate support.

0 Kudos
Reply