USBDM how print pcb image ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USBDM how print pcb image ?

2,101 Views
PO220
Contributor IV

Hello

 

Happy new year 2012

 

I'm looking for USBDM 4.7 but I don't understand how print the pcb image.

 

In USBDM_JS16CWJ.pdf file, pcb image is hidden by the names and housings of components.

 

thank you in advance

Tags (2)
0 Kudos
Reply
3 Replies

1,461 Views
pgo
Senior Contributor V

Dear petitours,

 

If you are referring to the PDF files, these are not intended for manufacture. They are assembly diagrams. They are not accurate enough to be used for producing a PCB. The component values etc are useful when assembling a board.

 

To print or arrange manufacture of a PCB the gerber files supplied separately should be used. PCB companies expect files in this format.

 

The original Altium designer files are also provided.  You can download a trial version of this software to use with these I believe,

 

If you want to print the Gerber files then there are a few free 'Gerber viewers' available that will allow you to do this.For example I've use 'gerbv' :

 

http://sourceforge.net/projects/gerbv/

 

 

bye

0 Kudos
Reply

1,461 Views
JulsPower
Contributor II

Where are those gerber files?

I just installed the msi file and no gerber available :S

0 Kudos
Reply

1,460 Views
ивандончев
Contributor I

USBDM - Browse /Version 4.10.0 at SourceForge.net

go on the link above
there are 3 folders -> go to Hardware
the gerber files are included in the .rar files

0 Kudos
Reply