USBDM driver for win10

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USBDM driver for win10

6,710件の閲覧回数
monstor
Contributor II

I can connect the USBDM with Codewarrior v5.1 in Win7. But now the USBDM cannot be detected in Win10 system. Should I have a USBDM driver for Win10?

タグ(4)
0 件の賞賛
3 返答(返信)

3,835件の閲覧回数
nkgavali1
Contributor II

My USBDM is detected in Win 10. But, I cannot see the USBDM option in connection list for new project in CW5.2.

0 件の賞賛

3,828件の閲覧回数
pgo
Senior Contributor V

Hi,

It's better to post a new query rather that ask at the end of an old (unrelated!) posting.

When using USBDM with codewarrior 5.2 you choose the TBDML target.

See this page: https://usbdm.sourceforge.io/USBDM_V4.12/USBDM_JS16/html/usage_page.html 

bye

0 件の賞賛

6,016件の閲覧回数
lama
NXP TechSupport
NXP TechSupport

Unfortunately, the CodeWarrior v5.1, is not supported by Windows 10. Please see the host platforms below.
  • Host Platforms:
  Windows® XP 32-bit and 64-bit (Professional Edition)
 Windows Vista 32-bit and 64-bit (Business)
 Windows Vista 32-bit (Home Premium)
 Windows 7 32-bit and 64-bit (Professional Edition)
 Windows 7 32-bit and 64-bit (Home Premium) 
  
  If you are using bellow platforms you need to use the CodeWarrior version 5.2.
  Microsoft Windows 8 32- and 64-bit
  Microsoft Windows 8.1 32- and 64-bit
  Microsoft Windows 10 32- and 64-bit

It is also good to look at following links if you will go to CW v 5.2.

https://community.nxp.com/message/1004832?commentID=1004832#comment-1004832 

Best regards,

Ladislav

0 件の賞賛