USBDM driver for win10

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USBDM driver for win10

7,614 Views
monstor
Contributor II

I can connect the USBDM with Codewarrior v5.1 in Win7. But now the USBDM cannot be detected in Win10 system. Should I have a USBDM driver for Win10?

Tags (4)
0 Kudos
Reply
3 Replies

4,739 Views
nkgavali1
Contributor II

My USBDM is detected in Win 10. But, I cannot see the USBDM option in connection list for new project in CW5.2.

0 Kudos
Reply

4,732 Views
pgo
Senior Contributor V

Hi,

It's better to post a new query rather that ask at the end of an old (unrelated!) posting.

When using USBDM with codewarrior 5.2 you choose the TBDML target.

See this page: https://usbdm.sourceforge.io/USBDM_V4.12/USBDM_JS16/html/usage_page.html 

bye

0 Kudos
Reply

6,920 Views
lama
NXP TechSupport
NXP TechSupport

Unfortunately, the CodeWarrior v5.1, is not supported by Windows 10. Please see the host platforms below.
  • Host Platforms:
  Windows® XP 32-bit and 64-bit (Professional Edition)
 Windows Vista 32-bit and 64-bit (Business)
 Windows Vista 32-bit (Home Premium)
 Windows 7 32-bit and 64-bit (Professional Edition)
 Windows 7 32-bit and 64-bit (Home Premium) 
  
  If you are using bellow platforms you need to use the CodeWarrior version 5.2.
  Microsoft Windows 8 32- and 64-bit
  Microsoft Windows 8.1 32- and 64-bit
  Microsoft Windows 10 32- and 64-bit

It is also good to look at following links if you will go to CW v 5.2.

https://community.nxp.com/message/1004832?commentID=1004832#comment-1004832 

Best regards,

Ladislav

0 Kudos
Reply