USBDM_JMXXCLD

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USBDM_JMXXCLD

1,000 Views
somy
Contributor I

Dear all,

I am new to OSBDM, I have purchased one USBDM_JMXXCLD and using it, it worked for two days, now pc is unable to recognise it, i have tried on different PCs, I have checked the power supply on controller pins it is ok, what may be the reason?

Thanks

sanjay

Labels (1)
0 Kudos
1 Reply

366 Views
pgo
Senior Contributor V

Hi Sanjay,

If it was working and now is not working it would seem most likely to be a hardware or mechanical problem with the BDM rather than a software one.  Especially if it doesn't work on other PCs.

For what it's worth you can try installing the latest drivers (not the applications) from Sourceforge as they seem a bit more reliable at installing but I would think it unlikely that it will make any change.

As you have only used the BDM for a few days I would suggest contacting the seller as it may be defective.

I have had no trouble with reliability except if used incorrectly e.g. excessive target power etc,

bye

0 Kudos