Hi,
I'm very new to USBDM and CodeWarrior. I've been tasked with updating an legacy product. I've been given a USBDMLT from TechnologicalArts.com and a licensed copy of Freescale Code Warrior 5.7, build 1932. Although the installed directory is "CW for HC12 V4.5", which makes it sound like it is Code Warrior V4.5 - so i'm already confused.
I've downloaded and installed the USBDM drivers, I've installed the standalone programs and can talk to the USBDM, which in turn can interogate the target processor (the detect chip button works). So i'm satisfied that it has installed correctly.
The problem comes when I try to use this within the HiWave debugger. Because the version of Code Warrior i'm using isn't recognised by the installation process of the USBDM program, the integration changes aren't made. This means the TBDML or Open Source BDM options aren't available when selecting a connection. I only get
Abatron BDI
HCS12 Serial Monitor
P&E Multilink/Cyclone Pro
Full Chip Simulation
SofTec HCS12
I've been reading a lot about various DLLs and getting the HiWave to talk to a new GDI DLL, but I don't know if this still applies or if it does, where to get it from. My client is not being a lot of help either, so I was really hoping someone here could point me in the right direction or simply tell me this isn't going to work and save days of hair pulling!
Thanks,
Andrew
Hi,
Thank you both for your replies. The special edition is too limited, the code is too large to use this version.
What I've ended up with is using the hiwave.exe from the special edition and loading the resultant .abs file into it. This seems to work OK and gives me the programming / debug facilities, while using the older Code Warrior version for editing and compiling.
Hopefully this method will see me through to the completion of this project.
Hi Andrew,
USBDM is not tested with that version of Codewarrior. This leaves you with a few alternatives:
Let me know how you go and if necessary I can try installer the earlier version if I can find a copy.
bye
i suggest you test the same with CW5.1 instead. here is the link to download CW5.1 special edition. http://www.freescale.com/webapp/sps/site/overview.jsp?code=CW_SPECIALEDITIONS