USBDM: Can´t "load and go" with MC9S08PA4,MC9S08PA8,MC9S08PA16,..

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USBDM: Can´t "load and go" with MC9S08PA4,MC9S08PA8,MC9S08PA16,..

734 Views
lucianonicolau
Contributor III

Hi PGO,

About HCS08 Programmer with USBDM_JMxxCLD: I´d like to understand why "load and go" does not work for MC9S08PA8. It load and can´t go (do not execute).

Where is the  XML that contain the address to start running? I see the "_entry_point" reset vector is 0xFFFE. It is the same of the others like QE8. Why QE8 works and PA8 does not work?

How to fix it?

0 Kudos
1 Reply

485 Views
pgo
Senior Contributor V

Hi Luciano,

I have located the problem and I expect it to fixed in the next version.

bye

0 Kudos