USBDM & 9S08SF4

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USBDM & 9S08SF4

Jump to solution
606 Views
ecb
Contributor II

Hi all,

I have a DEMO9S08SF4 board. I soldered the BDM connector as off my other boards.

My other boards work fine with the USBDM (4.10.6) under CW 10.3 (Win 7 amd64) but I have trouble with this DEMO9S08SF4:

sf4_4.jpg

I have problem also under Flashprogrammer with this board (Flashprogrammer work fine with my other boards):

sf4_5.jpg

Please I would appreciate any help ...:smileysilly:

Thanks!

0 Kudos
Reply
1 Solution
431 Views
pgo
Senior Contributor V

Hi ecb,

That's a rather nasty bug introduced when I added support for the PT devices.  Deleting one line was required!

Attached is an updated programmer file and GDI files.

Copy the .exe to C:\Program Files (x86)\pgo\USBDM 4.10.6.110 (or similar)

Copy the .dll to C:\Apps\Freescale\CW MCU v10.5\MCU\bin\plugins\support\HC08\gdi (or similar)

The latter files are untested.

Please let me know if this fixes the problems.

I will roll the changes into the next version.

bye

View solution in original post

0 Kudos
Reply
2 Replies
432 Views
pgo
Senior Contributor V

Hi ecb,

That's a rather nasty bug introduced when I added support for the PT devices.  Deleting one line was required!

Attached is an updated programmer file and GDI files.

Copy the .exe to C:\Program Files (x86)\pgo\USBDM 4.10.6.110 (or similar)

Copy the .dll to C:\Apps\Freescale\CW MCU v10.5\MCU\bin\plugins\support\HC08\gdi (or similar)

The latter files are untested.

Please let me know if this fixes the problems.

I will roll the changes into the next version.

bye

0 Kudos
Reply
431 Views
ecb
Contributor II

Hello pgo,


I love You ! :smileywink:

The problem is solved. Thanks so.

Some idea for my other problem with OSBDM ? (see CW 10.3 & DEMO9S08SF4)

Bye

C.B.

0 Kudos
Reply