USBDM 4.10.6 install fail on Windows 7 32-bit

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USBDM 4.10.6 install fail on Windows 7 32-bit

Jump to solution
606 Views
adamb
Contributor I

Hi,

I have a problem with installation of USBDM 4.10.6 package on Windows 7 32-bit. I have checked on two PCs with this operating system and it behaves the same. After window with installation options there is a popup:

USBDM_4_10_6_installation_problem.png

I have 4.10.5b version and it was installed without a problem. Of course previous version was removed before attempting to install 4.10.6.

Regards,

adamb

Tags (1)
0 Kudos
1 Solution
421 Views
pgo
Senior Contributor V

Hi adamb,

Yes I discovered this a little while ago.  One of the DLLs used by the installation has a dependency on a MinGW library.  This doesn't show up on my test machine as it has MinGW installed.

A corrected installer was uploaded a few hours ago.

bye

View solution in original post

0 Kudos
2 Replies
422 Views
pgo
Senior Contributor V

Hi adamb,

Yes I discovered this a little while ago.  One of the DLLs used by the installation has a dependency on a MinGW library.  This doesn't show up on my test machine as it has MinGW installed.

A corrected installer was uploaded a few hours ago.

bye

0 Kudos
421 Views
lucianon
Contributor I

Hi pgo,

The 4.10.6a still not working on win7 and winXP. I tried more than 5 PCs with no success.

The 4.10.5b works fine!!!

Tested with hardware USBDM_JMxxCLD.

bye

0 Kudos