USBDM 4.10.6.250a does not calculate/populate Trim Frequency values for Internal Clock Module

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USBDM 4.10.6.250a does not calculate/populate Trim Frequency values for Internal Clock Module

935 Views
MarcoAlvarez
Contributor I

Hi, I just upgraded from 4.10.4a to 4.10.6.250a, and found that the clock trimming calculations are not done automatically on the latest release.

I am using the HCS08 Programmer, on JM60, GB60, GT16A on Windows 7x64.

Was this feature discontinued? or is there a way to re-enable it?

Thanks,

Marco.

Labels (1)
Tags (1)
0 Kudos
2 Replies

544 Views
pgo
Senior Contributor V

Hi Marco,

It is not intentional.

I don't have ready access to the current release version.

The current development version seems to program the trim correctly on a GB60 device so I'm unsure if this problem doesn't occur with this version due to changes or simply is intermittent.

When you say it doesn't program the trim do you mean:

  • The trim option is disabled
  • The reported trim value is incorrect or missing
  • The value programmed to the device does not agree with the reported value

Also, what hardware are you using?

bye

0 Kudos

544 Views
MarcoAlvarez
Contributor I

PGO,

Thanks for your reply. I apologize for the delay. Yes, I meant that the trim option was disabled, and the trim frequency/value did not show when the checkmark was selected.

I am using an USBDM_JMxxCLD Rev1.6.

I also just built an USBDM_CF_JMxxCLD_V3 Rev 3.1.

I just upgraded to 4.11.1.60   (BDM FW4.11.1, and  DLL4.11.1.60), and everything is working fine using both devices. (for

Thanks again for all your help!

Marco.

0 Kudos