USBDM_4_10_6_220_Win.msi for CW 10.6 in Windows 7 64bit

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USBDM_4_10_6_220_Win.msi for CW 10.6 in Windows 7 64bit

Jump to solution
1,255 Views
stefanomanca
Contributor III

Hi, I want to use FRDM-KL25Z like a debbuger using CW 10.6 so  I installed USBDM_4_10_6_220_Win.msi and USBDM Drivers 1.2.0 but I get always "unknow device" instead no problem if I install USBDM 4.10.6.130 but in this case only Cw 10,5 could be used.

I'm getting crazy.

Any idea?

Thank you.

Stefano.

0 Kudos
1 Solution
739 Views
pgo
Senior Contributor V

Hi Stephano,

Could you install using the latest drivers available here (1.3.0):

http://sourceforge.net/projects/usbdm/files/Version%204.10.6/Drivers/USBDM_Drivers_1_3_0_Win_x64.msi...

Install USBDM (version 4.6.10.230 should be available shortly) :

USBDM - Browse /Version 4.10.6/Software at SourceForge.net

Update the firmware on the board to the version available in the BDM Flash Images.  See:

USBDM: Setting Up the FRDM-KL25Z

Plugin in the BDM and then check in the device manager to see what it says about the device.

bye

View solution in original post

0 Kudos
2 Replies
740 Views
pgo
Senior Contributor V

Hi Stephano,

Could you install using the latest drivers available here (1.3.0):

http://sourceforge.net/projects/usbdm/files/Version%204.10.6/Drivers/USBDM_Drivers_1_3_0_Win_x64.msi...

Install USBDM (version 4.6.10.230 should be available shortly) :

USBDM - Browse /Version 4.10.6/Software at SourceForge.net

Update the firmware on the board to the version available in the BDM Flash Images.  See:

USBDM: Setting Up the FRDM-KL25Z

Plugin in the BDM and then check in the device manager to see what it says about the device.

bye

0 Kudos
739 Views
stefanomanca
Contributor III

GREAT GREAT GRAT......IT WORKS

I love you, pgo.:smileyhappy::smileylaugh:

0 Kudos