USBDM_4_10_6_220_Win.msi for CW 10.6 in Windows 7 64bit

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USBDM_4_10_6_220_Win.msi for CW 10.6 in Windows 7 64bit

ソリューションへジャンプ
1,207件の閲覧回数
stefanomanca
Contributor III

Hi, I want to use FRDM-KL25Z like a debbuger using CW 10.6 so  I installed USBDM_4_10_6_220_Win.msi and USBDM Drivers 1.2.0 but I get always "unknow device" instead no problem if I install USBDM 4.10.6.130 but in this case only Cw 10,5 could be used.

I'm getting crazy.

Any idea?

Thank you.

Stefano.

0 件の賞賛
1 解決策
691件の閲覧回数
pgo
Senior Contributor V

Hi Stephano,

Could you install using the latest drivers available here (1.3.0):

http://sourceforge.net/projects/usbdm/files/Version%204.10.6/Drivers/USBDM_Drivers_1_3_0_Win_x64.msi...

Install USBDM (version 4.6.10.230 should be available shortly) :

USBDM - Browse /Version 4.10.6/Software at SourceForge.net

Update the firmware on the board to the version available in the BDM Flash Images.  See:

USBDM: Setting Up the FRDM-KL25Z

Plugin in the BDM and then check in the device manager to see what it says about the device.

bye

元の投稿で解決策を見る

0 件の賞賛
2 返答(返信)
692件の閲覧回数
pgo
Senior Contributor V

Hi Stephano,

Could you install using the latest drivers available here (1.3.0):

http://sourceforge.net/projects/usbdm/files/Version%204.10.6/Drivers/USBDM_Drivers_1_3_0_Win_x64.msi...

Install USBDM (version 4.6.10.230 should be available shortly) :

USBDM - Browse /Version 4.10.6/Software at SourceForge.net

Update the firmware on the board to the version available in the BDM Flash Images.  See:

USBDM: Setting Up the FRDM-KL25Z

Plugin in the BDM and then check in the device manager to see what it says about the device.

bye

0 件の賞賛
691件の閲覧回数
stefanomanca
Contributor III

GREAT GREAT GRAT......IT WORKS

I love you, pgo.:smileyhappy::smileylaugh:

0 件の賞賛