hi
I hope someone could help me, because I am blocked...
I need to use EVB Kit KIt912F634AVEVME and associated FreeMaster Interface.
the TBDML is well recognized by Win7. I follow all EVB documentation regarding setting , but it does not worked.
On the same EVB, I download a soft using CW5.X trough the TBDML , and it was working well.
But not way to use to the TBDML with FreeMaster.
I uninstall the TBDML driver.
And now, nothing work..neither the Freemaster neither trough CW5.1.
With CW, I got a window " USBDM Configuration HCS12" which pop.. ==> Failed to connect to target / reason : BDM open Failed - Unknown USB error.
With Freemaster , no connection => "could no open the communication port ...."
Thanks in advance for your help
I really appreciate
br
Vincent
official TBDML doesn't support 64bit win7.
But I ever had a customer successfully install TBDML on 64bit win7. this is the solution he shared to me. i never used it, but you could also try if you want.
1. install CW5.1 to 64bit win7 direcly
2. copy tbdml.dll to ...\prog\gdi.
3. remove tbdml.dll from C:\WINDOWS\system32
Hi Vincent,
TBDML is not USBDM. You appear to have installed USBDM. This may be conflicting with your use of TBDML. I suggest you uninstall USBDM. You may have to re-install CW just in case.
However, I don't think TBDML works under windows 7 anyway does it?
Do you have a link for a description of the hardware you are using?
bye