TBDML CodeWarrior V4.5 Special Edition

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TBDML CodeWarrior V4.5 Special Edition

8,709 Views
franz
Contributor I
Hi all together

I just finished the mounting of the TBDML.

With the Version 3.1 of CodeWarrior I am able to select TBDML in the Connection-menu of the debugger.And it seems that TBDML works.

But with the V4.5 Special Edition, I have only the options
Abatron BDI
HCS12 Serial Monitor
P&E Multilink
Full Chip Simulation
SoftTec HCS12
although the file "GDI.tgt" is in the prog.folder.

Could anybody help me to solve this problem.

BR
0 Kudos
Reply
6 Replies

1,842 Views
Alban
Senior Contributor II
Hello,
 
You can select a particular target by using SET GDI command in the command window.
 
Put the TBDML dll in the GDI dll folder as well and select it.
 
Alban.
0 Kudos
Reply

1,842 Views
franz
Contributor I
Hi Alban,

thanks a lot for the support. It´s not so easy to find that way for a newby.

BR

Franz
0 Kudos
Reply

1,842 Views
Alban
Senior Contributor II
Hello Franz,
 
That's true that all it's not very straight forward.
Because TBDML is a new thing, it is not included in CodeWarrior natively.
 
However the CodeWarrior team is taking this into account as I think they already included the OSBDM08 (for (R)S08) as standard target in CW for S08 v.5.
Hopefully it means that the next revision or Service Pack of CW S12 v4.5 will include the TBDML as native as well.
 
May be our Dear CrazyCat has an insider input on this :smileywink:
 
Anyway, DO FEEL free to ask your questions, there are a lot of people here eager to help !!!
 
Cheers,
Alban.
0 Kudos
Reply

1,842 Views
CrasyCat
Specialist III
Hello
 
Sorry I did not see that message before today.
In fact connection to TBDML cable will be available in CodeWarrior for HC12 V4.6.
 
As far as I know this release should be placed on the web soon.
You will then be able to select TBDML as connection when creating a project.
 
CrasyCat
0 Kudos
Reply

1,842 Views
franz
Contributor I
Dear Crasy Cat

this would help a lot for beginners. Because if you start with a project you can´t select TBDML as a target. You have to insert a target for TBDML and you should modify some settings, so that TBDML is started when you start the debugger. For example set TBDML.ini in the "Build Extras Arguments Menue. So not to do the same boring things all the time when starting the debugger.

Sorry for the late answer, but it took a lot of time to find out this things and find my error in the design. :smileyhappy: But now it works fine.

Thanks a lot
0 Kudos
Reply

1,842 Views
CrasyCat
Specialist III
FYI

CodeWarrior for HC12 V4.6 can be downloaded from following URL:

http://www.freescale.com/webapp/sps/site/overview.jsp?nodeId=01272600612247

Then click on

CodeWarrior Development Studio for HC12 Microcontrollers

CrasyCat

0 Kudos
Reply