RS08 Evalue8 Tool Schematic?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RS08 Evalue8 Tool Schematic?

8,794 Views
xwing
Contributor I
Hi,
 
I have received RS08 Evalue8 kit but there is no schematic documentation of the circuit board.
I tried connecting 12VDC to external jack and blown the JB16 chip.
 
Does anyone of you have schematic diagram of this 3rd party tool?
 
regards,
Xwing
 
 
Tags (2)
0 Kudos
Reply
6 Replies

2,699 Views
Pingu
NXP Employee
NXP Employee
Here's the Evalue8 schematic
 
Message Edited by t.dowe on 2009-10-26 05:28 PM
0 Kudos
Reply

2,699 Views
xwing
Contributor I
Thanks for help.
 
BTW, what are the available c-compiler for KA series MCU using codewarrior?
I heard that Codewarrior will have c-compiler ready early next year.
 
What about now? How to compile using 3rd party compiler like in-dart or pe micro?
 
regards,
Xwing
0 Kudos
Reply

2,699 Views
RockyRoad
Contributor III
Xwing -
 
Here is the schematic for the Evalue8 board.
 
- Rocky
 
Message Edited by t.dowe on 2009-10-26 05:30 PM
0 Kudos
Reply

2,699 Views
xwing
Contributor I
Thanks Rocky!
0 Kudos
Reply

2,699 Views
baddad
Contributor I
This looks like it has the OSBDM on-board. 
 
Do you know what software and driver they are using?
It should be open source as well.
 
Brian
0 Kudos
Reply

2,699 Views
RockyRoad
Contributor III
It's close to the OSBDM, but the Evalue8 board does require different dll's and firmware. The Evalue8 is not open source.
 
- Rocky
0 Kudos
Reply