Q>connecting the J3 of tbml to programm a uC?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Q>connecting the J3 of tbml to programm a uC?

5,991 Views
daistar
Contributor I
how will i connect the J3 fo tbml in order to program a uC?? like what are the pins description of the J3 and where to connect it in to a uC??? a schematic will be very helpful... tnx
0 Kudos
Reply
4 Replies

1,823 Views
daistar
Contributor I
what is EVB and tnx for replying.....
0 Kudos
Reply

1,823 Views
daistar
Contributor I
oh shoot...i'm sorry i've got confused of the word BDM.........just to clarify pin1 should be connected to BKGD/TAGHI/MODC...right? and pin4 to RESET..right? of 9s12dp512
0 Kudos
Reply

1,824 Views
DanielM
Contributor III
get yourself a schematic of an EVB. Essentially you are right, but you will also need pull-ups on both lines.

Daniel
0 Kudos
Reply

1,824 Views
Alban
Senior Contributor II
Hello,

If you read the TBDML_manual_15.pdf included in the archive...
Funnily enough, that is the User Guide and the Schematics !!!

Alban.
0 Kudos
Reply