Port to different processor

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Port to different processor

784 次查看
leb
Contributor I

In the not too distant future I want to be able to create projects using the Kinetis line of processors.  This means that I will need to build a new BDM as the first one I built lacks the requisite connector.  I wondered if, while I'm at it, I would port the BDM processor to, say, the MCF51JM60(pin compatible) and replace the USB stack with one of the freebie stacks from Freescale.  I wondered, however, if that is really a good choice since the SPI on the V1 processors supports only 8 bit transfers and it seems 9 bit would be better.  BUT, all the V2 processors seem to have only 1 SPI and the BDM appears to need 2.  Is there a Coldfire processor that has 2 SPI with variable data format that I didn't see?  Is the whole concept really worth the trouble?  Thanks for the feedback.

标记 (2)
0 项奖励
回复
0 回复数