P&E releases OSBDM design build v29.04

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

P&E releases OSBDM design build v29.04

1,318 Views
Zahar
Contributor IV

Hello All,

 

The latest OSBDM build version 29.04 has been released by P&E Microcomputer Systems. It includes Firmware/Drivers source files, circuit diagrams, BOMs, virtual serial port and firmware update utilities as well as a design guide. The latest OSBDM firmware and drivers support new features such as automatic firmware update (under Codewarrior 10.1 and newer), virtual serial port and trim for HCS08/RS08/CFV1 devices.

 

OSBDM build version 29.04 includes embedded support for HCS08, RS08, Coldfire V1, Coldfire V234, Kinetis ARM, HC(S)12(X), DSC, and Qorivva MPC55xx/56xx Freescale architectures.

 

To download the latest OSBDM design package and learn more about this embedded hardware interface, please go to:

 

http://www.pemicro.com/osbdm/

 

Best Regards

Zahar

P&E Microcomputer Systems.

Tags (2)
0 Kudos
Reply
1 Reply

448 Views
Pablin_83
Contributor I

Dear Zahar,

 

I wonder if you can solve my question in this post :

 

https://community.freescale.com/message/93606#93606

 

I want to know if Codewarrior 7.1 and 7.2 support OSBDM version 26, which is being required in order to work in CW 10, but I wouldn't want to lose contact in CW 7.1.

 

Your help will be really  appreciated,

 

Many thanks and regards,

0 Kudos
Reply