OSBDM can't work under CW3.1 ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

OSBDM can't work under CW3.1 ?

4,777件の閲覧回数
Jared
Contributor I
I have made a OSBDM board . but it can't work properly under CW3.1 .

It can't erase/program the HCS08's flash . How to do ?
ラベル(2)
タグ(2)
0 件の賞賛
返信
3 返答(返信)

1,153件の閲覧回数
lemonmeng
Contributor I
Please use CodeWarrio 5.0.
0 件の賞賛
返信

1,153件の閲覧回数
peg
Senior Contributor IV

Hi Jared,

Looks like the short answer is: Use CW V5.0, Its free from this site.

I just tried to use the OSBDM in V3.1 and it sort of works but you get a reduced menu in the simulator which does not include the "flash" option and the load dialog box does not have a load into flash option like in V5.0. There maybe a way to get it to work but this just looks like a great reason to upgrade to me.

You need an upgraded licence than what you get with the package to flash more than 1k. See here:

http://forums.freescale.com/freescale/board/message?board.id=8BITCOMM&message.id=744

BR Peg

 

Message Edited by peg on 04-21-200612:01 AM

0 件の賞賛
返信

1,153件の閲覧回数
Jared
Contributor I
I think if someone can give a license like CW5.0 ,OSBDM can work under CW3.1 just like CW5.0.



peg wrote:

Hi Jared,

Looks like the short answer is: Use CW V5.0, Its free from this site.

I just tried to use the OSBDM in V3.1 and it sort of works but you get a reduced menu in the simulator which does not include the "flash" option and the load dialog box does not have a load into flash option like in V5.0. There maybe a way to get it to work but this just looks like a great reason to upgrade to me.

You need an upgraded licence than what you get with the package to flash more than 1k. See here:

http://forums.freescale.com/freescale/board/message?board.id=8BITCOMM&message.id=744

BR Peg

Message Edited by peg on 04-21-200612:01 AM




0 件の賞賛
返信