Hi All,
I have been using the OSBDM build into the M52259DEMO board with CW7.1.2 for a couple of days to test out a couple of RTOS's. After erasing the flash memory one time I now get the error:
GDI Protocol PlugIn: The Debugger can not write memory.
It appears that it can read memory okay because checking the protocol log shows that the chip ID is successfully returned. Also, I went into the hardware diagnostics tool and found that I could read IPSBAR and RAMBAR and I could write to RAMBAR also.
The firmware in the OSBDM was v26, I found that it was a bit old so I've updated it to the latest with the new P&E tool but I still get the same error.
Strange as it was working fine earlier, is there some kind of lock to prevent a BDM writing to memory?
Here is the protocol log of a "blank check":
GDI: DiGdiOpen()
==> DI_OK
GDI: DiGdiVersion()
==> DI_ERR_NOTSUPPORTED
GDI: DiGdiAddCallBack(8192)
==> DI_OK
GDI: DiGdiAddCallBack(16384)
==> DI_OK
GDI: DiGdiInitIO()
GDI: Callback(DI_CB_MTWKS_EXTENSION) kind=MTWKS_CB_REPORTONLYFATALERROR, Result=DI_OK
GDI: Callback(DI_CB_MTWKS_EXTENSION) kind=MTWKS_CB_GETSTATUSWHENSTOPPED, Result=DI_ERR_NOTSUPPORTED
GDI: Callback(DI_CB_MTWKS_EXTENSION) kind=MTWKS_CB_COLDFIREAUTOCONFIG, Result=DI_OK
==> DI_OK
GDI: Reading From Memory Address: 0x04011000A, count: 2, memSpace: 2
GDI: DiMemoryRead()
==> DI_OK
GDI: 24 81
GDI: Writing To Memory Address: 0x020000000, count: 40, memSpace: 1
GDI: BC C5 BC C5 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
GDI: 00 00 00 00 00 00 00 00
GDI: DiMemoryWrite()
==> DI_ERR_FATAL
GDI: DiErrorGetMessage()
==> 1
GDI: Error Message ==> The Debugger can not write memory.
GDI: DiGdiClose(TRUE)
EDIT: I used the hardware diagnostic tool to read from 0x0401D0008 which is the SCFMSEC — CFM Security Register and it reads 80 00 FF FF which suggests that there is no flash security.
Any ideas??
Shaun