OSBDM and BeeKit

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

OSBDM and BeeKit

1,485 Views
quevedo
Contributor V

I have an e-value-8 board, and I have been using it with success to program a small board with a HC08JM. Now I got a kit with 2 boards for Zigbee development. Each board has a zigbee transciever and a HC08QE128, with the 6-pin BDM header. I have used the Beekit to generate code for a simple wireless UART test, and I have exported that code to CodeWarrior 6.2. When generating code inside beekit, the software asks the board I am using, so I have defined the board I have (MC1320X-S08QE128-EVB). When I select debug, what opens is the PEMICRO Connection Manager, with options to Cyclone and Multilink programmers, but no options for OSBDM. In the original window, the MCP tab has the board name as the only option in the drop-down box.

 

Does anyone know how I can configure BeeKit and/or CodeWarrior imported project to accept the OBDM as a programmer option?

 

Thanks in advance

 

Antonio Quevedo

Tags (2)
0 Kudos
Reply
0 Replies